The Example program has a default control panel built-in to make it easy to start an application.
Perform the following steps to operate the control panel:

The KAS Simulator displays the status and position of the axes.
It also displays the log messages.
Figure 10-38: Display of KAS Simulator
You can continue to use the Control Panel to:
To exit Simulation mode, do as follows:


For additional information about Kollmorgen Automation Suite, see the following documentation:
|
Copyright © 2015 Kollmorgen™ |
|